This website requires JavaScript.


휴일 안내: JLCPCB 공장은 5월 1일부터 3일까지 3일간 휴무입니다. 이 기간 동안 주문은 가능하지만, 배송 일정은 이에 따라 지연될수 있습니다.
자세한 휴무 일정은
여기에서 확인하세요>


Optimizing KICad Designs for JLCPCB Fabrication

블로그  /  Optimizing KICad Designs for JLCPCB Fabrication

Optimizing KICad Designs for JLCPCB Fabrication

Jan 10, 2025

KICad is making sure that your printed circuit boards (PCBs) can work with fabrication services, it is an important part of creating them. KICad is an open-source PCB design tool that has many features that can help plans work better with JLCPCB fabrication. This article will discuss into detail about methods to improve KICad designs. It will cover important topics such as design rules, choosing the right components, and getting the files ready so that the fabrication process with JLCPCB works efficiently.


Understanding KICad and JLCPCB


KICad is a powerful program that lets users make schematics, layout designs, and fabrication files for creating PCBs. JLCPCB offers low prices and quick response times, as it is a well-known PCB manufacturing service. It is important to know both what KICad can do and what JLCPCB needs for production in order to get the best results.


Design Rules for JLCPCB Fabrication


When making plans for the JLCPCB, it is important to follow certain rules:


Minimum Trace Width and Spacing:


JLCPCB tells you the minimum trace widths and spacing based on the PCB thickness you choose. The smallest distance for both is usually 6 mils (0.15 mm). In your KICad design settings, you should always check these criteria.


Layer Count:


JLCPCB lets you choose from different layer counts, but for easier designs, using fewer layers is better. Most of the time, a two-layer PCB is enough and will not cost too much.


Drill Sizes:


Verify whether the drill sizes of your design meet JLCPCB's standards. Common lengths are 0.4 mm, 0.6 mm, and 0.3 mm.


Component Selection


Picking the right parts is important for making your idea work better. Take these things into account:


SMD vs. Through-Hole Components:


Surface-mount devices (SMD) are typically better than through-hole components in terms of size and performance when deciding which one to utilize. Make sure that the chosen parts can be used with the ways that JLCPCB makes boards.


Library Management:


To keep correct component footprints, use KICad's library management. This helps avoid problems during the building and putting together processes.


PCB Layout Tips for JLCPCB


For efficient fabrication, it is important to have the right PCB layout. These are the best ways to do things:


Proximity to Power Pins:


To reduce noise and voltage changes, put parts like resistors and capacitors close to the power pins of integrated circuits. This makes the device work better.


Component Grouping:


Put together parts that are related to make the layout easier and improve the integrity of the signals. Putting parts together based on their role can make routing and putting them together easier.


Thermal Management:


Make sure there is enough space between parts to keep them from getting too hot and keep their performance at its best. Thermal vias and heat sinks can help get rid of heat even more.


Preparing Fabrication Files


A very important part of the planning process is making sure you have the right files for JLCPCB:


Gerber Files:


KICad can send out Gerber files, which are the usual format for making PCBs. Make sure you include all the layers you need, like the top, bottom, solder mask, and stencil.


Drill Files:


Along with Gerber files, make a drill file (Excellon format) to show where and how big the holes are. This is an important part of making the PCB.


Assembly Files:


If you are using SMD parts, you might want to make an assembly file that shows where the parts should go. This makes putting things together easier, especially for bigger projects.


Simulation and Testing


It is important to simulate and try your PCB layout before you finalize your design.


Electrical Rule Check (ERC):


To find any problems in your circuit design, run an ERC in KICad. Before making something, this can help find mistakes.


Design Rule Check (DRC):


Do a DRC to make sure that your plan follows the JLCPCB design rules. This helps keep expensive mistakes from happening during production.


Submitting Your Design to JLCPCB


Once your plan is ready and optimized, sending it to JLCPCB only takes a few easy steps:


Upload Files:


Go to the website for JLCPCB and share your Gerber and drill files. Make sure that all the relevant files are included.


Select Options:


Pick the details for your PCB, like the material, width, color, and number of boards. Look over all of your choices to make sure they meet your style needs.


Review and Order:

Make sure all the information is correct before you place the order. This step can help the building process go more smoothly and save time.


Post-Fabrication Considerations


Following your PCBs from JLCPCB, there are a few crucial tasks you need to do:



Visual Inspection:


Extensively review the PCBs to ensure that every component is in the correct location and that no clear issues exist.


Testing:


Functional testing helps you make sure that the device operates how it should. This helps figure out if there were any problems during creation.


Documentation:


For future use, keep detailed records of your plan, files for making it, and test results. This can be very helpful for fixing problems and making designs over and over again.



Go Ahead of the game with JLCPCB rapid PCBA solution

Conclusion


PCB making must include optimizing KICad designs for JLCPCB fabrication. You can speed up the fabrication process by knowing the rules for design, choosing the right parts, and following best practices for planning and file preparation. Following these tips will not only make your PCBs more reliable, but it will also help your electronic projects run more smoothly and efficiently.


As technology keeps getting better, ideas that work well will become even more important. Designers can make high-quality PCBs that meet the needs of current electronics by using KICad's features and JLCPCB's services.


JLCPCB Quote

Recent Posts