How to design JLCPCB layout using KiCad
How to design JLCPCB layout using KiCad
Creating a Printed device Board (PCB) layout is an important part of making sure that an electronic device works and is reliable. Many people know that JLCPCB is a good company that makes high-quality PCBs. KiCad is an open-source PCB design tool that both pros and amateurs use a lot. You can make accurate and useful PCB layouts by mixing JLCPCB's services with KiCad's powerful tools.
The steps in this article will show you how to use KiCad to design a JLCPCB layout. We will discuss about the most important steps, best practices, and tricks for getting the most out of these tools so you can make PCBs that work well and are stable.
What is KiCad?
For electronic design automation (EDA), KiCad is a set of free software programs. Helps in making schematic designs and turning them into PCB layouts for production. The modular structure of KiCad lets users create schematics, organize components, run models, and see 3D images of the final PCBs. There are more and more people using it, it is free, and it has many tools for different PCB creation needs.
Key Features of KiCad:
- Schematic Capture
- PCB Layout
- Library Editor for components
- 3D Viewer for PCB visualization
Error finding tools include Design Rule Check (DRC) and Electrical Rule Check (ERC).
Understanding JLCPCB
JLCPCB is one of the top PCB producers; they produce reasonably cost, premium PCBs. Beginning engineers and professionals utilize JLCPCB for prototypes and small-scale manufacturing since it offers various customizable options and fast turnaround times. It is easy to use them for a variety of projects because they can handle different PCB thicknesses, finishes, and solder mask colors.
Why Choose JLCPCB?
Prices that are easy on the wallet for samples and small runs.
Made with high quality materials and a range of choices for board thickness, layers, and finishes.
Fast shipping times and the ability to make prototypes quickly.
Support for and a lot of different ways to change SMT assembly.
Preparing for PCB Design: Components and Layout Strategy
To avoid mistakes and problems in the PCB layout, it is important to do the right research before starting the design process. Here are some things to think about:
Component Selection:
First, make sure you have all the parts you need for your plan. Make sure that every part in KiCad's library has a matching footprint, like resistors, capacitors, integrated circuits (ICs), and connections. If not, you might need to make your own tracks.
Schematic Design:
Draw your circuit design in KiCad's schematic editor. This is where you indicate how electrically linked parts are. KiCad makes it easy to place symbols and route wires to show how parts relate to each other.
Design Rules and Constraints:
It is important to make sure that the design rules, like trace width, spacing, and layer layout, are in line with what JLCPCB can make. JLCPCB gives design rule guidelines for different types of PCBs that should be followed to make sure the boards can be made.
Component Placement Strategy:
It is very important to think about where to put components like surface-mounted devices (SMDs) and through-hole components when making a PCB plan. A well-planned and sensible placement of components guarantees proper signal routing, effective thermal management, and lessened noise interference.
Step-by-Step Guide to Designing JLCPCB Layout Using KiCad
Step 1: Schematic Design in KiCad
To start, open KiCad's design editor and add the parts that you need. Make sure to:
Make sure the part numbers and symbols are correct.
Use lines and buses to properly connect the parts.
Give each part a unique name so there is no misunderstanding later.
To make sure there are no mistakes in the design, use KiCad's electrical rule check (ERC).
After you finish the schematic, you need to make a netlist, which is the file that links the schematic to the PCB plan.
Step 2: Creating the PCB Layout
Once you have the netlist, go to KiCad's PCB layout tool and begin putting parts on the board. When you load the netlist, all the parts will be available to put on the board. Here are some planning tips that will help you:
Proximity to Power Pins:
To reduce noise, put parts like decoupling capacitors close to the power pins of integrated circuits.
Component Grouping:
Put together parts that are related, like SMD capacitors, to make routing easier and keep the signal's integrity.
Thermal Management:
Make sure heat-sensitive components have enough room to prevent them from getting very heated.
Ground Plane Design:
Design for a solid ground plane on one of the layers to reduce noise and improve power distribution.
Step 3: Routing the Traces
Routing is the process of using copper lines to connect the parts. KiCad lets you choose between automatic and custom routing. When setting up:
For high-speed signals, keep the lines as short as possible to cut down on parasitic inductance.
To cut down on electromagnetic interference (EMI), do not cross signal lines.
To make sure the board can be made properly, follow JLCPCB's design rules for trace width and spacing.
To make sure that your wiring follows the rules and there are no shorts or unconnected pins, use KiCad's Design Rule Check (DRC) tool.
Step 4: Adding Vias and Layers
To connect traces between layers on boards with more than one, add vias. As stated in their instructions, make sure that the via sizes are within the range of what JLCPCB can manufacture.
Step 5: 3D Visualization
See what the PCB will look like with KiCad's 3D viewer once you have completed the design. This guarantees that there are no technical issues and that the parts are in their correct location. You can also use the 3D view to show your idea to clients or other team members.
Step 6: Generating Gerber Files
PCB makers use Gerber files, which are the standard format, to make the boards. Go to "Plot" in KiCad and export the Gerber files, making sure to include all the layers you need, such as copper, solder mask, silkscreen, and so on.
Also, make the drill file, which shows where all the holes are on the board and what size they are.
5. Submitting Your Design to JLCPCB
Go to the JLCPCB website and send your files once the Gerber files are ready. JLCPCB allows you to obtain an instant provide by defining board size, thickness, number of layers, and finish. Once you know the price, place the order and see the manufacturing process through to completion.
6. Best Practices for JLCPCB Layout Design
When using KiCad to create a PCB for JLCPCB, keep these best practices in mind:
Use Design Rule Check (DRC):
Run the DRC in KiCad often to find any mistakes before making Gerber files. This helps manufacturers avoid problems that might happen.
Check JLCPCB’s Capabilities:
Always look at what JLCPCB can make, like the smallest trace width, via size, and spacing. Following these rules will make sure that the producing process goes smoothly.
Optimize Component Placement:
Place the components including integrated circuits (ICs), resistors, and capacitors such that routing is simpler and signal integrity issues are minimized. Keep high-frequency components close together and ensure integrated circuits (ICs) are near decoupling capacitors.
Thermal Relief:
Make sure that parts that make heat have enough thermal relief. Adding thermal vias and thinking about heat sinks for high-power parts are two ways to do this.
Conclusion:
Using KiCad to design a JLCPCB layout is a structured process that needs careful planning, placement of components, and routing techniques. By following the steps in this guide, you can make PCB designs that are efficient, easy to make, and meet both functional and performance needs. Using KiCad's flexibility and JLCPCB's production services together will lead to excellent results, no matter if you are making simple single-layer boards or complicated multi-layer designs.
It will become more and more important for engineers, designers, and beginners to learn how to use PCB design tools like KiCad and services like JLCPCB as the need for smaller, more efficient, and more powerful electronics grows.