PCB Milling for Prototyping: Fast, Accurate, and Cost-Effective Solutions
PCB Milling for Prototyping: Fast, Accurate, and Cost-Effective Solutions
The method of PCB milling is to remove copper portions from a fully copper board to replicate pads, signal tracks, and designs. The design patterns and structure are planned under a GBR G-CODE layout file. Similar to etching this is also a subtractive process, hence create the circuit by removing copper material from the board. PCB milling does not involve any chemical methods, making it suitable and safer for use in general home or office environments without the need for handling hazardous chemicals.
High quality circuit boards can be produced using either process. Unlike in the etching process the quality factor of a PCB is determined by mask dimensions, state of the etching chemicals and photolithographic steps. Here in milling the quality factors are milling accuracy, control system, sharpness and rotational speed of the milling bits. In this article we will determine the hardware, software requirements, design parameters and factors to keep in mind while performing PCB milling. To see how JLCPCB made their PCBs, here is our ultimate design guide blog.
The Design Parameters of PCB Milling
The spacing between adjacent tracks and trace width is determined by the milling tool diameter. The tool diameter is the lowest 0.1 mm, the normal diameter ranges from 0.1 to few mm. Usually the best possible feature size we can get in the industry standard process can go up to 0.254mm in the case of CNC and 0.127mm in the case of laser engraving method. Depending upon the milling tools and hardware setup max error in design can be determined. Here are the list of different milling tools used in the process:
1. End Mills
Flat End Mills: Used for cutting straight paths and removing large areas of copper.
Ball End Mills: Ideal for contouring and shaping complex surfaces.
2. V-Bit Engravers
These are used for fine detailing and for creating intricate copper trace patterns. They work well for small and precise cuts but might not be as effective for larger copper removal.
3. Drill Bits
Used to drill through-hole pads and vias to establish connections between PCB layers.
4. Engraving Bits
Engraving bits create shallow grooves for marking labels, component outlines, or even for creating very fine isolation paths between traces. They can be essential for boards where space is tight.
5. Slot Cutters
These tools are used for creating slots for components or for cutting the outline of the PCB itself, useful for boards that need irregular shapes.
6. PCB Routers
These are used for the final outline cut, separating individual PCBs from a larger panel after all traces and drilling are complete.
Hardware Setup for Milling:
A PCB milling system is a single machine that can perform all of the required actions to create a prototype board, with the exception of inserting vias and through hole plating here are the full details:
Mechanical system:
The mechanics behind a PCB milling machine are fairly straightforward and have their roots in CNC milling technology. A CNC milling machine consists of a 3D chassis, some motors, chuck bolt and controlling mechanism. You will find a main drilling bit motor attached to the spindle. Which has speed ranges from 30,000 RPM to 100,000 RPM depending on the milling system. Then some X-Y-Z position control motors, usually stepper motors, are used for this purpose due to their high accuracy. The control mechanism has a microcontroller unit, a user interface and some speed control drivers. Positioning information and machine control commands are sent from the controlling software to the machine’s microcontroller via a serial port or parallel port connection. Here are some details about the X-Y-Z positional control.
X and Y-axis control:
For the X and Y-axis drive systems most PCB milling machines use stepper motors that drive a precision lead screw. A lead screw is a big bolt at which the base of a CNC plotter is mounted. Copper board is attached to the base and then X-Y motors move the base according to the software setting. The spindle motor position is fixed during this. The speed of PCB design is the function of X-Y-Z control and spindle speed.
Z-axis control:
The first and most common is a simple solenoid that pushes against a spring. When the solenoid is energized it pushes the milling head down against a spring stop that limits the downward travel.
Software of CNC PCB Milling:
When it comes to PCB CNC milling, a range of specialized software is available to handle tasks like PCB layout design, G-code generation, and CNC control. Here's a breakdown of the types of software used at each stage:
1) PCB Layout Design Software: To create the actual PCB design, including traces, pads, and layout details. Some online free solutions are KiCad, Eagle and EasyEDA.
2) CAM (Computer-Aided Manufacturing) Software: Converts PCB designs (usually Gerber files) into G-code, which CNC machines use for milling. Some solutions include: FlatCAM, CopperCAM and Autodesk Fusion 360.
3) G-Code Sender / CNC Control Software: Sends the G-code to the CNC machine and controls the actual milling operation. Example GRBL Controller and Universal Gcode Sender (UGS).
The Advantages of PCB Milling
PCB milling offers advantages for prototype production and certain specialized PCB designs, with the biggest benefit being the absence of chemicals involved in PCB fabrication. PCB milling has advantages for both prototyping and some special PCB designs.
CNC machine prototyping can provide a fast-turnaround board production process without the need for wet processing. When creating a prototype, outsourcing a board takes time. An alternative is to make a PCB in-house. Using the wet process, in-house production presents problems with chemicals and disposing thereof.
Applications of PCB Milling:
The applications are not only creating copper onto the copper panel but it can also prepare the full PCB with cut-out, milling slots, V-scoring, separating panels and cutting heat sink cavities. A single machine could carry all the parts of the process drilling, milling and cutting. A PCB milling machine can be a good solution to test your prototype designs faster. So that after proper prototyping and tests we can get our hands on professional PCB from a manufacturing company.
- Cut-out
- Milling slots
- V-scoring
- Separating panels
- Cutting heat sink cavities
Milling VS Etching:
Milling: A CNC machine physically carves out copper like tiny jackhammers on your board. Perfect for anyone who likes noisy machines doing the work for them. It is good for larger traces, but it may not handle ultra-fine details. It produces copper dust, which is easy to clean in comparison with chemical processes. It is fast, especially for one-offs. Perfect if you need a prototype yesterday.
Etching: A chemical bath eats away unwanted copper. Just a little chemistry experiment, no big deal, unless you hate dealing with chemicals. It is good for detailed work and complex designs. It becomes less safer due to involvement of hazardous chemicals. It takes longer with setup, but smooth for high-volume runs if you have the patience.
Conclusion:
In conclusion, PCB milling provides a straightforward, efficient way to produce quality prototype boards in-house without the hassle of chemicals or waiting for outsourcing. Milling offers control over designs and allows engineers to perfect layouts, ensuring compatibility before mass production. This approach is particularly valuable for rapid prototyping, quick adjustments, and immediate testing all crucial steps before scaling up.
Once you've validated your design and tested the prototype, it's time to consider professional production for larger quantities. JLCPCB offers high-precision PCB manufacturing services to bring your final designs to life at scale, whether it's for small batch runs or full production. With JLCPCB's quality assurance and industry-grade fabrication, you can be confident that your design will be manufactured accurately, meeting both your specifications and performance expectations.
Recent Posts